Part Number: OPA855
Other Parts Discussed in Thread: OPA847, OPA140
Hi,
We have received inquiry that customer having issue in the output for OPA855, please see details below.
"
I am trying to build an optical homodyne detection system, see the Kumar et al. (2012) paper for our inspiration basic design layout.
We originally built a TIA with a gain of 4.99 kV/A following the specs laid out in this paper, but we needed a TIA with a gain of 100 kV/A, with an ideal bandwidth of 10 MHz. So, we switched the op-amp from OPA847 to OPA855 for the high GBWP.
However, somewhere along the way, the changes introduced oscillation in the output of the TIA. To confirm that this was not simply a problem from the high gain. I changed the feedback resistance to 11.7kOhm on both the old and the new board. The results show that the OPA847 still performs without oscillations while the OPA855 does.
Note that the photodiodes (PDs) are inserted using PD sockets and the photodiodes can be removed at any time this leaves the TIA with no input and even under these conditions we see that the OPA855 oscillates. The supply is a Keysight precision DC source, so it should be stable. And I did make some tests with EM shielding and it did not help the OPA855 circuit.
The PDs that I am using have a parasitic capacitance of 8 pF each.
Details are shown in the attached PowerPoint presentation. Also, the KiCad files for the OPA855 board are all in "Homodyne Detector. zip".
Any and all input would be welcomed.