This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH7220: IN+ / IN- current draw outside of 4V differential

Part Number: LMH7220

Looking for some help clarifying the input current draw (e.g. impact on a reference voltage supply) for something like a mid-point supply on Vin- and a full-range swing at Vcc=12V (Vin+_min = 0V; Vin+_max = Vcc-2 = 10V; Vin- = fixed 5V)

Figure 4 shows the input current going exponential as the diff hits about 3V:

I realize that this shows an approx. differential input impedance of 320k, but want to be sure I understand the part's performance outside of that linear region at the center.

Thanks