Hello
I have several questions for device
When the upper OP-AMP is a normal Vcc input and the lower OP-Amp is an abonormal Vcc input, the voltages at points 1 and 2 are not equal. Can leakage occur at the input of OP-AMP when the components power is not supplied?
If I use the LT1014MJB(DIP) package type,can the voltages at points 1 and 2 be the same?
Are the input characteristics of SMD Type and dip type devices different?