This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA849: INA849 output is severely offset

Part Number: INA849
Other Parts Discussed in Thread: LM358, REF4132

With Vref 2.5V, the output should normally fluctuate up and down with 2.5V as the center.

Now the bad problem: when the input is below 4mV, the output is centered at 2.5V,

The larger the input amplitude is, the more obvious the output shift is. When the input reaches 10mV, the shift is about 1V.

Please help analyze the possible reasons and design instructions for related problems.

Input differential mode Common mode and power supply are within Diamond Plot safe range

 power supply :+/-10V