Hi,
I am using your product "TLV9352" for the following application.
Purpose:voltage follower
Supply voltage:+12V, GND
Under the above conditions, is there a possibility of damage if the input voltage is indeterminate?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using your product "TLV9352" for the following application.
Purpose:voltage follower
Supply voltage:+12V, GND
Under the above conditions, is there a possibility of damage if the input voltage is indeterminate?
What exactly do you mean with "indeterminate"?
A changing input voltage is no problem. (And input voltages near V+ are no problem either.) But the inputs should always be driven to some voltage, i.e., the inputs should not float. Otherwise, extreme input voltages could make the amplifier go into a saturated state (see section 7.3.8 of the datasheet).
If it is possible that there is no signal source, you can add a weak voltage divider (e.g., 1 MΩ + 1 MΩ) to ensure that the input voltage is always biased somewhere.