Other Parts Discussed in Thread: INA326, ADS1294
Hi,
I am designing an EMG amplifier using the INA326 as the differential input component. I have referred to many of the forum posts involving the design of EMG/ECG amplifiers but still I am unsure about a couple parts of the design.
1) Design for Single Supply
I intend to power the INA326 using Vcc = +5V and Vss = GND. Am I correct that I then must bias reference pin 5 to Vcc/2? Also are there any impedance requirements for pin 5? I plan to derive Vcc/2 using a buffered op-amp configuration for low output impedance.

2) I am using a cascaded low-pass and high-pass filter for the following stage and with the output from the INA326 at Vcc/2 subsequent filter op-amp stages are biased to Vcc/2. I am getting a bit confused in terms of knowing how to handle COM of the patient, GND of the sensor/amplifier board (Vss for INA326 and filtering op-amps) and the reference voltage Vcc/2 that the EMG signal will ride on. Currently I plan to use a driven right leg configuration to set the COM potential of the body to Vcc/2 and provide high common mode rejection for 60 Hz noise. A reference schematic of the setup is included below. I have not optimized the feedback loop of the DRL yet to improve stability. Do I have the basic configuration correct? And is my methodology of driving the body potential to Vcc/2 since it is used as the common of the INA correct?
3) In terms of the INA326 bias currents currently the only path is from ground through the body and through the electrodes. I did not want to provide an additional path to GND (VSS) on the inputs as that would degrade input impedance. Will the output of the INA326 saturate if the electrodes are not connected to the body and bias path is not provided? Or does the driven right leg circuit provide an additional bias path for the INA326? A reference schematic of the INA portion is provided. Do I need to provide any additional considerations for accommodating the bias currents required by the INA326?
Thanks,
Chris Wiebe