Hi Team,
Our customer is looking for the comparator with SC-70 package and below pin-outs, can you help to check if we have such device? Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no comparator with this pinout.
Either hand-solder the devices dead-bug-style, or create a new board.
Hello Jacky,
This is the older, rare "LMC7101" pin-out, where the supplies are reversed from the standard "NorthWest" pinout.
The only comparators with this pinout are the LMC7211, LMC7215, LMC7221, LMC7225 and TLV7211.
Unfortunately, none are available in SC-70. I'm guessing they are using the ON NCS2202... AFAIK, it is the only device with that pinout/package combo.