Other Parts Discussed in Thread: TLV3402
Hello,
I have a question regarding the TLV7042. I have the two TLV7042 comparators acting as a window comparator. Vx (labeled on the schematic below) can have a voltage from 0-12V. In order to protect the input of the window comparator when Vx reaches above the absolute maximum input rating of the comparators, R39-3 and D5-3 were added to "clamp" Vin to 4.7V in such an event. However, D5-3 has enough reverse leakage current that Vin is pulled below the 4V window comparator threshold even when Vx is ~5V.
Long story short, I am wondering if the inputs to the TLV7042 would still be protected if I removed D5-3 and kept R39-3? The datasheet mentions the input terminals are "diode-clamped to VEE", but does not mention any diode clamping to VCC. Are there any internal protections here that would allow me to simply remove D5-3, or will I have to find a less-leaky diode?
Thanks,
Grayson Capers