Part Number: TLV9052
I have validated our circuit design using the TLV9052IDR package. I will probably use the TLV9052SIDGSR because a complete CAD model is available for this version of the TLV9052.
There don't appear to be any different electrical characteristics between the two options. However, TLV9052SIDGSR has a shutdown line for each op-amp. Do I just tie these to pin 10 (VCC) to prevent an accidental shutdown if they are left floating? Later we might find that this shutdown feature is useful since this is going on a battery-powered agricultural field system so this SIDGSR may be a better choice in the long run.