This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2316: Vout from negative rail

Part Number: TLV2316

IF the TLV2316 is powered with a 0 to 5V supply ( V+ = 5V and V- = 0V (GND) ) and the input (+IN A) is also connected to ground (0V) and -IN A is tied to OUT A (unity gain configuration), what would be the output offset on OUT A from the negative rail (GND)?  I am observing OUT A is equal to 0V with no offset from the negative rail.

THanks