This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm facing issue related to noise and voltage hunting at AMC1200 and OP-AMP output.
Please check the schematic if any thing is wrongly connected.
R20-2Mohm,R22-2Mohm and R24-1Kohm
C20-10nF,C22-0.1uF,C24-0.1uF
R342,R346-3K3,R347,R343-5K6,C229-1nF
Hello Mahesh,
The negative output of the AMC1200 should not be directly connected to ground as connected. The outputs are driven and when connected in this way, damage to the device may occur.
I recommend taking a look at the differential to single-ended conversion in this document for an example: https://www.ti.com/lit/an/sbaa347/sbaa347.pdf
Hello Alexander,
Okay I understand. Is there any chance, voltage will be unstable/hunting on secondary side with this type of configuration.
Hi Mahesh,
yes, of course, because you short circuit one output of the AMC1200 !!!!!!! A differential amplifier has to be connected to the output, or an ADC with differential inputs.
Kai