This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA855: How can I achieve High Gain BandWidth TIA

Part Number: OPA855



Hello,

We are developing a light communication system including IR LED and photo diode. An OPA855 is used as a TIA in and some photo diodes have been checked such as BPW 34S and BDP-C107. We would like to achieve a frequency response of 50-60MHz.

 

The simulation in LTspice shows the 3dB frrequency over 100MHz but it is about 20-25MHz in the actual test! Can you help me on this issue?

One IR LED (SFH 4715AS) is used as a transmitter and one OPA855 evaluation board coupled with PD is used as a receiver.

 

Thank you