Part Number: INA281
Hello,
I'm using the INA281 to monitor a 1 mA current source with a 10 ohm sense resistor, producing an offset of 10mV that is then amplified by 500 V/V. It is in the high side current sense configuration with a load of 100 ohms. The common-mode voltage is about 0.1 V. I will include a schematic of my sensing circuit to this post.
I'm in the process of completing an error analysis for my circuit, and I was wondering how I should compute the error for....
- The ideal offset vs. the offset resulting from input bias currents of the CSA.
- The ideal load current vs. the load current resulting from the input bias currents of the CSA.
Thank you so much.