I am using the INA321E, powered by a single ended 3.3V supply. I intend to apply a small differential signal at the inputs (~1mV) biased by a common mode voltage, centered within the allowable input common mode range.
According to the INA321 Datasheet, the output is Rail-to-Rail, and should be able to go within 50mV of the Rails.
But according to the Analog Engineer's Calculator "Vout Max" is limited to 2.1 Volts, even though the supply is 3.3 Volts (please see attached PDF).
So according to the Data Sheet, I should bias my input signals by 1.65 Volts, but according to the Engineer's Calculator I should bias my input signals by about 1.2 Volts - which is correct?
Also, please confirm that INA321 Vout can go to 3.250V, not the 2.1V indicated by the Engineer's Calculator.
Thanks for clarifying the situation here. If there are any dependencies or conditions that factor in, please explain, thanks.