Other Parts Discussed in Thread: ADC104S021,
Hi TI
Circuit function: The operational amplifier (LMC7101AIM5/NOPB/SOT23-5/TI) is designed to follow the circuit to sample ADC and monitor the change of voltage.
Phenomenon: during the test, it is found that the output voltage signals of the 10 prototypes of the R&D prototype are normal (normal in normal temperature and high temperature environment tests); However, in the small batch stage, all the output signals of the op amps in the 10 prototypes showed oscillation waveforms (see the figure below), and the higher the temperature, the higher the amplitude of oscillation. The circuits and PCBs of the two batches are identical.
The customer did the ABA test, and the abnormal phenomenon followed the bad film. Please help analyze the cause.
In addition, we found that the silk screen of the defective products was inclined. Will this happen in our production stage?