Other Parts Discussed in Thread: OPA990, TLV6001
Since LMC7101 is an old part, customer wants to check whether there is any new recommend part? The voltage supply is 12V. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Aki,
Just beware that the power supply pins of the SOT-23 LMC7101 are reversed compared to the standard "Northwest" SOT pinout.
The newer SOT-23 devices are not drop-in compatible and may need a re-layout. Be sure to verify the pinout of any selected replacements.
I do not see any current 12V devices with the correct pinout at this time.
The upcoming TLV6001 has a "R" version with correct "reversed" pin out (TLV6001RIDBVR), but is only 5.5V supply max. The Amplifiers product line can advise if they have anything in development with this pinout.