This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6881: Need the gain information at 2150 MHz for single ended input with 5V supply voltage

Part Number: LMH6881
Other Parts Discussed in Thread: TINA-TI

Need the frequency versus gain plot for the above mentioned part number for single ended input signal with input impedance of 50 ohm and supply voltage of 5V. 

Thanks in advance

  • Hello Sujoy,

      Unfortunately, we do not have a measured AC response of single-ended input. But, this measurement should be very similar to specified in the datasheet (Figure 1) with higher gain of 26.6dB if both feedbacks are kept symmetrical and the input common-mode voltage is within range specified in device datasheet (2.5V). 

      Here is simulated single-ended data which shows similar results: 

      Tina-TI file attached below.

    LMH6881.tsc

    Thank you,

    Sima