This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: 4GHz FDA at Gain 10.4dB

Part Number: LMH5401

Hi,

Our customers are looking for a fast FDA that can be used under the following conditions.
Can I use the LMH5401 as a candidate?
It looks difficult because the small signal response is 6Ghz.


Power supply voltage = 5.0Vpp (supplied from LDO)
Input signal amplitude = 600mVpp (fixed value)
Output signal amplitude = 1200mVpp~2000mVpp (to be adjusted during evaluation)
Gain=6dB~10.4dB (Value converted to GAIN of output signal amplitude)
Input/output frequency 4GHz

Please let me know if there are other good products.

Best regards,

Hiroshi