Other Parts Discussed in Thread: TLV4021
Hi ti team,
I configure two TLV7021s as fig 40 in datasheet to implement over volt and under volt protection to the PCBA's main power. TLV7021 is supplied with 3.3V. Later I will adjust R1,2,3 for the proper Vth+ and Vth-.
These is a issue: the main power is normal +12V and the circuit should be able to detect up to +17V for OVP. Both 12V and 17V excess the VCM of 7021.
Can volt divider to be used to decrease the main power to the range in VCM? That means the input of Window Comparator will be divided by two resisters through the main power. I am not sure the the impedance of the IN+ and IN- high enough to the volt divide resisters.
Thanks to your reply.