This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I would like to connect two INA819 amplifiers in series to achieve high bandwidth and high gain. Attached is the Tina simulation.
Side notes:
R3 and R5 put some load on the OpAmps. I thought at best this was necessary. But it doesn't seem to change anything.
The gain is set to about 28.7 for each OpAmp.
If there is no connection between the two INAs, everything works as expected. However, the series connection leads to distortions in the simulation. Is this just simulation artefacts or a problem? Solutions?
It seems the simulation is somewhat unstable anyway. If I add low-pass filters, I often get convergence errors.
Your help is much appreciated.
Thanks and best regards
PatrikINA819_Offset_v1.TSC
Patrik,
That is correct - the resistive loading does not effect the gain unless resulting the output current exceeds the short-circuit limit.
In AC simulation I see expected -3dB and -6dB bandwidth of around 1MHz - similar what datasheet shows (see below).

As far as 'distortion' of the cascaded INA819's, I believe they are transient simulation artifacts - see below.

No problem. Running discrete transient simulation using ideal op amps shows all nodes operating in linear region well within the supply voltage - see below.