Other Parts Discussed in Thread: AMC1350, AMC3330, ISO224, AMC1351
Hi,
I'm trying to perform a DC voltage measurement with the AMC1350, but I'm having some difficulties:
I have a resistive divider to measure a DC voltage link. I would like to measure the voltage across one of the intermediate resistors of the resistor divider (a resistor that is not present at the edges/ends of that divider).
Employing the AMC1350, for some reason I could not perform the measurement on an intermediate resistor that I would like to do. The AMC1350 only measured the voltage when I replaced the resistors at the bottom with a short circuit (so that the resistor where the measurement takes place was connected to the negative pole of the DC link).
The figure below illustrates what I said:
All the documentation I found indicates to connect GND1 to the negative side of the measured voltage, without a resistor.
Would it be possible to use the AMC1350 in my first setup (without the short circuit)?
If yes, how? If not, why not?
Thank you in advance,
Regards.