Hi there,
I just want to check is that possible INA240A1 can be used in this condition:
Vdc=48V
Current sensing type: 3phase inline current sense
Shunt resistor: 3mohm*2 in parallel
Maximum continues current: 110A
Maximum pulsed current: 200A @1ms
If those conditions is not recommand use INA240
Could you recommand another solution for those condition?
Thanks
Kevin