This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA564-Q1: What's the output peak current?

Part Number: OPA564-Q1

Hi  team,

could you help to check what's the output peak current? and what's the test condition?

thanks 

  • Hi Hazel, 

    could you help to check what's the output peak current?

    The output peak current is specified at 1.5Apk, typical, which are tested at Tamb = 25C. 

    I realized that the datasheet did not specify the output current is DC or AC at 1.5A. The OPA564-Q1's actual operating current is determined by the SOA curve, shown in Figure 46.  

    If you are able to provide me with design requirements, I can simulate the worst case condition and check out the power dissipation on the part. 

    Best,

    Raymond