Could you please tell me if the input stage of OPA2188 is FET or Bipolar?
Also, are there any common and general ways to distinguish these two kinds of stages?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you please tell me if the input stage of OPA2188 is FET or Bipolar?
Also, are there any common and general ways to distinguish these two kinds of stages?
The OPA2188 is a chopper amplifiers with auto-calibration frequency of 650kHz - thus, its input stage is implemented with CMOS transistors. However, it input stage uses back-to-back input protection diodes (see below) that may become forward biased with large step input signal or when output is pushed against one of its rails.