Part Number: PGA309EVM-USB
Other Parts Discussed in Thread: PGA309
Hi Team,
PGA309EVM-USB EVM and sboc320c are being used.
The customer is testing with the three temperature (-40°C, 25°C, 70°C) calibration process of the PGA309, the hardware is in current loop mode and is sampled using the internal TEMP ADC.
Issue: Data below 0°C cannot be written to EEPROM, calibration data above 0°C is normal.
Could you please help check this case? Thanks.
Best Regards,
Cherry