This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kind of scanning through the OPA828 datasheet (2022 update) this plot
So that Aol over temp plot should say 1/Aol and I really doubt it flips polarity over temp
That 1/Aol going negative is basically saying the Aol phase is flipping around 180deg which should produce an oscillator going cold - probably really does not do that and this plot is getting mired with measurement noise.
Michael,
You are correct - since zero-crossing around 55 deg C in AOL vs Temp graph would implied infinite AOL, the negative numbers should have been taken absolute values of for the purpose of generating the graph. Thus, the actual graph may look more like the one shown below:
ABS value? really it is just your input err signal is lost in the noise not inverting polarity. Your redrawn suggest the Aol is going way up going cold, really? Not that important of a graph, but just misleadiong right now.
Assuming that he noise had been completely filtered out, the zero-crossing in AOL vs Temp graph implies some DC error that has NOT been calibrated out. As far as according to my redrawn graph AOL getting highest at cold, the graph is just a typical curve that may significantly vary from unit to unit.