Part Number: BUF802
Good day.
A question on the BUF802 noise. I desire to provide a noise match to the BUF802 and maximize SNR, hence minimize NF.
The model appears to support my calculations very well and operates as expected.
In the data sheet there is Figure 6-19 which provides the desired optimal noise resistance to 100 MHz.
I need to extend this data set to 500 MHz. The voltage noise appears flat at ~ 2.3 nV/root Hz, but the
noise current is rising quickly above 20 pA/root Hz.
Can you provide the noise V and noise I values at 500 MHz? And perhaps provide a curve set that fills the void 100-500 MHz?
Thanks! Alan Victor