Other Parts Discussed in Thread: TLV1701
Hello,
What would be the output of TLV1704 if there is no supply voltage to device.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I tried to simulate situation when TLV1701 has zero supply voltage. I used Pspice for TI.
Result is that the output voltage drops to zero.
Is this the true behavior of TLV1701, or just a problem with simulator.
Attached my DSN.
Hello Avinoam,
Vcc=0V is not a valid operating condition. The model is confused.
The output will be "high", as Clemens suggested, as there is no voltage to turn on the output transistor.
I cannot get into details, but there will be some current (~100nA) between the output and the supply that is not shown in the schematic due to ESD protection.