Other Parts Discussed in Thread: TLV1822
Dear Friend
When I tried setting a narrow hysteresis (400mv) with TLV1822, I wondered if a non-zero Low output of TLV1822 should be countable, the difference seems quite big.
I have Vcc = 3.3V, Vth = 1.5V, I want a 400mV hysteresis which means Vthh = 1.7V, Vthl = 1.3V. Assuming R3 is a pull-up resistor.
From the equations given by the datasheet, I got R1 = 0.1333 * R2, R3 = 0.2 * R2, if I let output Low equal to zero.
While I will get R1 = 0.16 * R2, R3 = 0.44 * R2, if I count 0.25V as the device output low. The two results showed a quite big difference.
Considering the datasheet said: "the pull-up resistor be at least 10 times less than the feedback resistor value", neither result will allow me to choose R3 like that...where should I go? What is the correct selection right now?
is there something wrong with my calculation? Or is it because 400mV hysteresis is too narrow with 250mV low output counted?
Anything enlightening me will be greatly appreciated.
Regards
Tony