Part Number: INA125

I'm using INA125 to read a 350 Ohm Load Cell. This is the circuit I'm using.
I assembled 10 circuits, and while 8 of them are working fine, 2 of them seem to have a value drift that accumulates to few Volts within 2 hours.
I tried connecting to unloaded Load Cell, to make sure it's not caused by load cell creepage. I also tried lowering the LC driving voltage from 10V to 5V, to decrease self heating by the current through the LC.
I measured the output at point A, so I know it's not caused by the second stage. I Also made sure with 0.1mV accuracy voltmeter, that the supply voltages, the LC drive voltage and the zeroing voltage, are all stable.
Made some exchanges between the good and bad circuits, also replaced the chips with new ones, and still the issue was not resolved.
Any other suggestions?