Hello,
I using INA193 to measure current from isloated power line.
INA193 is connected to 5V in V+ pin, GND to V-.
Vin + and Vin - are connected with 20m oHm resistor, the ground reference of Vin + and Vin - are not the same as GND, it called RTN_IN

Is this connection right ?
There is no data on isolation between ground, except CMR (data show 80dB).
Best Regards,
Yossi