This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Input Voltage: 60 VDC
Maximum Continous Current: 60A
I am using INA193 for the current measurement.
Please review my schematic.
your earliest reply will be highly appreciated
Regards
MurthyCurrent Shunt Monitoring.pdf
Hello Murthy,
Please note the error you will get from the input filtering. Also why use the second stage gain and not use the gain of 50 options? Another suggestion is you could use the INA293 or the INA290 which will have better accuracy.
Also the INA290 and INA293 do not have the under 20mV input voltage error explained in the INA193 device.