Other Parts Discussed in Thread: TLV2371-Q1
Hi,
Since TLV2371MDBVREP is EOL, can you suggest an alternate part number for this?
Thanks
Shihab.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Since TLV2371MDBVREP is EOL, can you suggest an alternate part number for this?
Thanks
Shihab.
The nearest replacement would be the TLV2371-Q1, but it is not identical.
Hey Shihab,
Thank you for posting on e2e.
Could you tell us more about the application's requirements?
We have the following EP devices in the TI portfolio in single channel DBV - 5:
All the best,
Carolina
Hello Caro,
Supply voltage requirements: >= 10V
Input Common mode range: Vcc (this component will be used at Highside)
Input voltage range: 0V to 1V
Channel count requirements: 1
Bandwidth: >3MHz
Thanks
Shihab
Hey Shihab,
Is the extended temperature range necessary (-55C to 125C)?
We have a lot more options available at -40C to 125C
Is it required to be an "EP" device?
Can you explain this part again?
Supply voltage requirements: >= 10V
Input Common mode range: Vcc (this component will be used at Highside)
Input voltage range: 0V to 1V
Channel count requirements: 1
The device does not require RRIO since the supply is larger than 10 and the input is 1V, there are 9V of headroom. Unless the input signal is 9 to 10V?
Here is a parametric table not considering the package restriction earlier:
There's 31 available options arranged price from lowest to highest: https://www.ti.com/amplifier-circuit/op-amps/products.html#78=In%20to%20V%2B%3BIn%20to%20V-%3BNo%3BOut&480=1&1192=-55%3B125&1261max=10%3B180&23typ=3%3B8000&sort=1130;asc&
All the best,
Carolina