Other Parts Discussed in Thread: OPA2333-HT, OPA211-HT, OPA2211-HT
Hi Team,
Is there TI solution to replace ADI AD8634HRZN? AD8634HRZN temperature is -40C to 175C, however OPA2210IDR only up to 125C.
Please suggest. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Is there TI solution to replace ADI AD8634HRZN? AD8634HRZN temperature is -40C to 175C, however OPA2210IDR only up to 125C.
Please suggest. Thanks.
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the single channel version of the OPA2211-HT. If a single channel option is reasonable this device might work. The OPA2333-HT does go to 210C, and it is also a dual, but this device has a 5V power supply. I will let the systems team know that there is a need for a dual precision high temperature op amp, but currently I do not think there is a good dual channel match.
Best regards, Art