Dear all,
I want to choose an accurate vale for an isolation resistor for my OP-AMP (OPA838), based on the datasheet OPA838 is very sensitive to capacitive loads and for make the system robust to instability we need to add an isolation resistor to the OP-AMP output, as we can with and without this resistor, there is an huge difference in the frequency response of the close-loop system:

For choosing the isolation resistor value, datasheet suggested this figure:

My question: is this parameter the close loop gain? if yes, if I have a different gain than, what I can see in the figure, how should I choose the isolation resistor? for example 60dB-> 1000 V/V?
My OPA838 configuration is transimpedance amplifier and the loop gain is 60dB-> 1000 V/V, so I wonder how can I choose this value?
My design: