Part Number: VFC32
Hi support team all.
We have received a question from our customer as below.
Question 1: When used with Voltage-to-Frequency,
Is it possible to control the frequency in 0.001V steps in the input voltage range of Vin from 0 to 10V?
Example: Vin:5.001, 5.002V...→50.01kHz, 50.02kHz
Question 2: If Vin cannot be controlled in 0.001V steps, please tell us the resolution at which Fout can be controlled relative to Vin.
<Circuit concept>
R1: 40kΩ, C1: 330pF, C2: 1000pF
⇒Vin:5V=50kHz, 10V=100kHz
I would like to control the frequency in 0.001V steps using the above concept.
Best regards,
Higa