Other Parts Discussed in Thread: TINA-TI,
Hello,
using Tina-TI, I'm running AC analysis for this fairly simple circuit. Its *.tsc file is attached below.

According to application note SBOA325, capacitor C1 provides a high-frequency feedback path that bypasses the transistor T1.
To see the influence of C1, I'm sweeping its value from 3nF to 6nF during AC analysis.
AC analysis shows: When C1 is < 5nF, the phase starts at +180°. For C1 >= 5nF, the phase starts at about -180°. I wonder why this is?
Is this a property of OPA172 or is it just a Tina-TI simulation quirk (e.g., "phase wrapping", as +180° and -180° are basically equivalent)?
Thanks.
Dan