Part Number: INA180
Tool/software:
Hi,
I have the attached implementation, where there are different grounds connected to INA180A1IDBVR device.
VCC3V3_IO's reference ground is GND.
Signals entering pins 3&4 have reference ground as Input_GND
The two grounds are connected together with 4 parallel beads (each 26ohms) elsewhere on the board. Will there be any impact to the circuit's working because of usage of 2 gnds?