This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I have the attached implementation, where there are different grounds connected to INA180A1IDBVR device.
VCC3V3_IO's reference ground is GND.
Signals entering pins 3&4 have reference ground as Input_GND
The two grounds are connected together with 4 parallel beads (each 26ohms) elsewhere on the board. Will there be any impact to the circuit's working because of usage of 2 gnds?
Hi,
I agree with Clemens - as long as the two are electrically connected, which is the case here, the device will work properly.
Regards, Guang