Part Number: THS4521
Tool/software:
hello,
I used THS4521 to make a single-ended differential circuit, the circuit is as shown below, and I encountered a problem during the test.

When I use the DC power supply to supply the IN+ input, I find that when the input voltage is less than 1.6V, the DC power side current shows a negative value,and sometimes the input is not equal to the output.when input is greater than 1.6V and the displayed current is postive,the output of the ths4521 is equal to input,and no abnormal phenomenon occurs.

When the input is floating, the differential output is above 1.6V. I added an op amp in front of the single-ended input as a follower, and then connected to the THS4521 IN+ and it didn't have this phenomenon. Is this normal? Why is this happening?