This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We are planning to use INA180A1DBVR for high end current sensing of 12V rail. The 12V is taken to a DC-DC convertor which generates 3V3 to the system.
The IN+/IN- of INA180A1DBVR are connected across the current sense resistor on the 12V rail. When the DUT is powered the IN+/IN- of the device will see a voltage before the device itself
will get power on the Vs pin. The datasheet seems to suggest this is ok to do so - but can I get a confirmation that it is ok to supply common mode 12V to the IN+/IN- lines when the device itself is not powered?
thanks
Yes; the absolute maximum ratings allow up to 26 V at the inputs under all circumstances. Also see figure 7.21.
Clemens,
Thank you for your correct reply per usual.
Hello Ranjeet,
Thank you for your post; Clemens is correct as this device can withstand your 12V present on the inputs before the supply is on for the device. This is a robust device and I completely understand the need for confirmation.
Best Regards,
Joe