Other Parts Discussed in Thread: INA226, INA238, INA228
Tool/software:
Would you have any suggestions for modifications to the schematic?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sky,
Thank you for using the TI forum. Here are my comments for your schematic:
Regards,
Mitch
Thank you for your response. The schematic has been updated as described below:
Model: INA226-Q1, Shunt Resistor: 1mΩ,
- UIC2619, Function: Exterior Lighting - Reverse Light Power (Lamp), Maximum Current: 0.33A
- UIC2729, Function: Exterior Lighting - Rear Fog Light Power (Lamp), Maximum Current: 0.2A
- UIC2730, Function: Exterior Lighting - CHMSL Power Supply (Lamp), Maximum Current: 1.8A
We have also added 2.2K pull-up resistors to the I2C lines.
Do we need to adjust the shunt resistor value? Are there any other suggestions?
Sky,
Thank you for your patience. Mitch is out of the office today but will reply when he returns on Tuesday.
Louis
Hello Sky,
With a 1mΩ shunt resistor, here is the required measurement range for each device:
- UIC26190: 0.33mV
- UIC27290: 0.2mV
- UIC2730: 1.8mV
For each of these, this is a very small percentage of the device full scale range, which is ±81.92 mV. This will make measurement accuracy very low, and I recommend increasing the shunt resistor size. Similarly, if you plan to use the current result register, then this shunt value will not work because the calculated calibration value to put in the register would be too large to fit in the register (increasing the shunt resistor would help with this also). Here is a link to an app note and calculator tool that can help you pick a better shunt value for your application:
https://www.ti.com/lit/pdf/sboa511 (App Note)
https://www.ti.com/tool/download/SBOR021 (Calculator Tool)
Regards,
Mitch
Hi Mitch
I have modified the shunt resistor values according to the documentation:
- UIC2619, Function: Exterior Lighting - Reverse Light Power (Lamp), Maximum Current: 0.33A: 20mΩ
- UIC2729, Function: Exterior Lighting - Rear Fog Light Power (Lamp), Maximum Current: 0.2A: 20mΩ
- UIC2730, Function: Exterior Lighting - CHMSL Power Supply (Lamp), Maximum Current: 1.8A: 10mΩ
Is there anything else that needs to be corrected in the circuit?
Sky,
Again, thank you for your patience. Mitch is currently out of the office but will reply as soon as he returns Wednesday.
Thanks,
Louis
Hey Sky,
Those shunt resistors will still be too small. I recommend using our error calculator tool to find a good balance between acceptable error and shunt resistor size, that can be found here:
https://www.ti.com/tool/download/CS-AMPLIFIER-ERROR-TOOL
Also, you may be interested in using the INA228 or INA238 instead. These devices are footprint compatible with the INA226, but have a lower input bias current so they will be able to measure small currents more accurately.
Regards,
Mitch