This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA821: Design review and question

Part Number: INA821
Other Parts Discussed in Thread: TMS320F28386D, OPA1637

Tool/software:

Hi,

We would like our INA821 design to be reviewed:

The input signal characteristics are the following:

  • Frequency: 1kHz to 15kHz
  • Voltage: ±1V to ±10V

This then feeds the CMPSS of a TMS320F28386D for frequency measurement using the CLB.

I also have a question, we are being asked if this would be compatible to acquire a single-ended 4V square wave, with negative input being connected to the GND.

From my understanding of the datasheet, I feel like this would be problematic as this would lead to unbalanced inputs as per requirement for Input Bias Current Return Path.

Best regards,

Clément