This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Poonam,
Abs Max junction temp would be 150°C.
However, proper operation is NOT guaranteed, only that the die is not damaged and will recover when brought within operation range.
Warranted operation is within the specified operation temp range of -40 to 85°C.