Part Number: INA500
Other Parts Discussed in Thread: REF2025, OPA365, REF2030
Tool/software:
Dear supporter:
In our design, We are trying to using INA500C to measure battery voltage, with 1.25V reference..
and found it accuracy performed quite good, up to 0.02% after calibration, when battery voltage is from 0.5V to 2.5V.
However when the battery voltage higher than 3V, accuracy drops, even worse when bat voltage goes higher such as 4.7V, the offset is more than 20mv, and cannot be calibrated because offset is not linear..
DC source was used to simulate battery, but we also tried with actual battery (100AH), same performance.
the reference is from REF2025, whose 1.25V o/p is buffered by OPA365.

Is there limitation for INA500C ? any suggestions?
Regards.
Qingfeng