Other Parts Discussed in Thread: TLV3801
Tool/software:
Hello, TI engineer.I followed the instructions to power up the chip, but IN sense could detect the signal I input, but out did not output a signal。
I have thought about possible issues:
1.When powering up the chip, I connected the positive pole of power supply 1 that powers VEE and the negative pole of power supply 2 that powers VCC together. I don't know if this is correct or not
2.The manual mentions“Verify that cables connecting to IN1+_SENSE, OUT1+, and OUT1- are matched length and impedance.Perform any de-skewing if necessary. Set the function generator (50-Ω terminated) to produce a square wave output with 400mVpp at 10 MHz, with a 0 V DC offset. Disable the signal generator output. Connect the signal generator output to IN1+.“,
I don't know what this matching length means? But my in1+dsense has output, so why isn't out+/out - outputting? What voltage does 400mVPP refer to?
3.If my chip is broken, how can I test if my chip is broken? What caused its damage? During the process of powering up the chip, current limiting was carried out according to the instructions, and the power of the input RF signal was below -10dBm
THANKS.