Part Number: OPA541
Tool/software:
hello.
I configured a paralled operation circuit with reference to Figure.15 in the Application of OPA541.

+VS: +6V, -VS: -6V
R1: 10K, R2: 10K
I set the input power to -1V and set the 5A in the loader instrument, it will be 1V/5A setting in the output.
Current Sharing of Master Opa541 and Slave Opa541 work well
but
I set the input power to +1V and set the 5A in the Loader instrument (polarity change), the output is -1V/-5A setting.
Current Sharing of Master Opa541 and Slave Opa541 do not work well.
The Master OPA Output Voltage starts with -1.45V and Slave -1.0V, and after about 30 seconds, it changes the same to 1.0V and 1.0V.
I want to check if this is normal.
And additionally 10A output is not available on SOA in that paralled operation circuit(+6Vs, -6Vs, 1Vout)? Is it possible up to 7A?