THS7530: THS7530 LTSpice Simulation

Part Number: THS7530
Other Parts Discussed in Thread: TINA-TI, OPA855

Tool/software:

Hi all,

I am interested in using the THS7530 as a programmable gain amplifier for our application.  I am using LTSpice 24.1.4 as I'm more familiar with LTSpice

The simulation circuit is as shown below:

Unfortunately the simulation just hangs including whether or not I skip the DC operating point calculation.

I would appreciate any help on getting this simulation working.

The simulation file is attached belowTHS7530 Simulation.zip


Thanks,


Sojhal

  • Hi Sojhal, 

    Our TINA-TI simulator is free to download at this link: https://www.ti.com/tool/TINA-TI

    I would strongly recommend simulating this model with TINA as TINA has a strong convergence engine and we have verified the model functionality using the TINA simulator. 

    Best, 

    Jacob 

  • Hi Jacob, thanks for the advice, I found the issue and it was very stupid, the input is floating and not ground referenced.  The result is slightly different than what TINA-TI gives you, for example in the lowest gain setting on LTSpice I got 8.6 dB, but in TINA-TI I got around 10 dB, whereas the DS specifies the lowest gain as being 11.6 dB.  I can live with those discrepencies however with TINA-TI the circuit simulation file seems to become irreversibly corrupted when I tried to build an analog chain consisting of a TIA (with an OPA855) and this PGA (THS7530).  

    I have documented that issue on another post on E2E:

    e2e.ti.com/.../5671189

    Thanks for your help

    Sojhal 

  • Understood. Thanks for the update Sojhal. I will support the debug on the other thread. 

    Best, 

    Jacob