Tool/software:
Hello,
In Figure 14 on page 17 of the Design Guide: 400-W Continuous, Scalable, +/-2.5-to +/-150-V, Programmable Ultrasound Power Supply Reference Design (TIDUCD8.pdf), there is a table for VOUT-P1 (V) and VCON-A1 (V); it shows that for VOUT-P1 = 150V, VCON-A1 is 5V.
Should VCON-A1 be 4.83871 V (=150*10k/310k) when VOUT-P1 = 150V? Thanks.
Best regards,
Mark Liang
Hi Mark,
Should VCON-A1 be 4.83871 V (=150*10k/310k) when VOUT-P1 = 150V?
Yes, your calculation is correct. The voltage divider at pin3 of TLV171UDBVR is (10/310)*150 = 4.83871V, and the U2 circuit is an integrator
But VCON-A1 is controlled by DAC, which is defined 5V by DAC.
If you have additional questions, please let me know.
Best,
Raymond
Hi Raymond,
Thank you for your reply.
What are the reason for VCON-A1= 3.22581V and 1.6129V, when VOUT-P1=100V and 50V respectively in Figure 14?
Best,
Mark
Hi Mark,
These are the voltage divider calculation based on the figure 14.
If you have other questions, please let us know.
Best,
Rayond