Part Number: USB2ANY
Tool/software:
03/25/2025
Dear Forum,
we have sereral USB2ANY Devices here. Our Development Laptops are Windows 11, the technical PCs where they are used, are WIN10.
We also have the Software TICS Pro Software.When installed and first plugged in, the TICSProsuggested a Firmware update which was done on the devices. This is a few days/Months back. The firmware updates were not performed by me but by any colleague. I do not know the actual firmware versions applied therefore.
When plugged in, the tics Pro sw can be started, a server started, for instance on <ip>:11000, on the test machines it is 127.0.0.1:11000. Then we use the python software snippets, that enable us to connect to this server as a client. Then there are some functions we can call, for instance reading out the serial numbers with the GetAllUSB2ANY() function. It returns with no error, by repeating the command and true, but the list with serial numbers of the devices attached is an empty string. NO serial numbers are reported! If we plug two such devices to a pc, where our python snippets run, we get the serial number of one of the two devices attached, i.e. the number of this one that has not been grabbed by the TICS Pro software. I we select the other of the two devices within the TICS Pro software, the game is switched... we get the serial of the first one that is now not being attached to the software. Also we do not see these devices in the device manager (how should they be visoible at all?).
How can we get the serial number read out with the GetAllUSB2ANY() function?
Thanks and warmest regards,
Roland